FB#.RESREFPHASE

Description

This parameter sets the electrical degrees of phase lag in the resolver.

See the motor resolver datasheet for the value for this parameter.

Context

See Feedback # View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

electrical degrees

Range

-180 to 180°

Default Value

-2°

Data Type

Float
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
FB1.RESREFPHASE

3500h

05h

Signed32

-

1000:1

Read/Write

No

FB2.RESREFPHASE

3501h

05h

Signed32

-

1000:1

Read/Write

No

FB3.RESREFPHASE

3502h

05h

Signed32

-

1000:1

Read/Write

No

FB4.RESREFPHASE

3503h

05h

Signed32

-

1000:1

Read/Write

No

FB5.RESREFPHASE

3504h

05h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

FB1.RESREFPHASE

30160

75D0

Signed32

Read/Write

-

FB2.RESREFPHASE

30161

75D1

Signed32

Read/Write

-

FB3.RESREFPHASE

30162

75D2

Signed32

Read/Write

-

FB4.RESREFPHASE

30163

75D3

Signed32

Read/Write

-

FB5.RESREFPHASE

30164

75D4

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

FB1.RESREFPHASE

30160

Float

Read/Write

-

FB2.RESREFPHASE

30161

Float

Read/Write

-

FB3.RESREFPHASE

30162

Float

Read/Write

-

FB4.RESREFPHASE

30163

Float

Read/Write

-

FB5.RESREFPHASE

30164

Float

Read/Write

-